View as Webpage

SEPTEMBER 2023 EDITION

 

Hello [First Name] !

Thanks for reading the September 2023 edition of Omron Electronic Component's product newsletter, Component Insider.

If you have any feedback on this new resource, please email us!

 

Sincerely,

The Team @ Omron Electronic Components

 

Featured Products 

G9KB

 

In the world of electronics, there's a growing need for energy solutions that are both efficient and durable. 

The OMRON G9KB Power Relay is designed for high-capacity applications as a solution to the growing need in the energy industry. A key feature of the OMRON G9KB is its ability to bi-directionally switch loads up to 50A at 600VDC. This is ideal for charge/discharge applications that would otherwise require multiple relays for each function. The G9KB is also designed with a low contact resistance of ≤5 mΩ, ensuring a lower heat generation when the high level load is passed through the contacts. This can potentially reduce the need for heat mitigation elements in the end product The OMRON G9KB meets the UL 60947-4-1 and EN 61810-10 standards, requirements for use within energy storage system devices. The OMRON G9KB Power Relay offers strong performance and follows important safety regulations, making it reliable for many applications.

 Learn More 

D2LS

 

The OMRON D2LS switch features a compact size and surface mount design, making it ideal for space-constrained applications. One of the standout features of the OMRON D2LS switch is a stable and clear click sensation. This tactile feedback ensures that users can push the switch with confidence, knowing that their input has been registered. The D2LS maintains a high level of responsiveness, ensuring that devices respond promptly to user. The D2LS is known for its exceptional endurance, and can withstand extensive usage cycles, ensuring longevity and consistent performance over time without losing its quality. The OMRON D2LS is a compact, durable switch that offers a clear click feedback button with quick response time when pressed, a great choice for applications requiring high durability and high operating force such as gaming controllers and mice. 

 Learn More 
 

OMRON News

The Expanding Landscape of Energy Technology 

The energy industry is undergoing a significant shift towards sustainability and technological integration, driven by environmental needs. OMRON's electronic components are pivotal in this transition, offering solutions for solar energy, advanced weather monitoring, and modern grid systems. OMRON solutions, including relays, sensors, and switches not only optimize energy harnessing and conversion but also adapt to real-time environmental changes, ensuring maximum efficiency. Especially in the rapidly growing electric vehicle market, OMRON guarantees efficient power management. These innovations are integral in achieving a balance in modern grid systems, ensuring seamless integration of various energy sources. As the challenges of transitioning to sustainable energy intensify, OMRON's pioneering solutions offer a clear path forward. Explore these groundbreaking technologies with OMRON today, steering our world towards a brighter and more sustainable energy future. 

Learn more

Fresh On The Board

Learn about our Ultra Subminiature Basic Switches and how their excellent operability and toughness are the keys to superior remote operation and control in our latest edition of Fresh on the Board.

Learn more

GGB: Gaming Supplier Showcase

Check out our GGB Supplier Showcase where our business development manager, Patrick Lahey, talks about the eye-catching See Through Panel technology from Omron. Patrick will break down the details of the STP’s features and capabilities, as well as the company’s impressive collaboration process that moves seamlessly from idea to prototype to mass production.

Learn more
 

 Upcoming OMRON Events 

INDUSTRY TECH DAYS:
HUMAN VISION SENSING TECHNOLOGY

OMRON’S 300A, 1000VAC PCB RELAY – G9KA-E 

Please join OMRON on October 3rd to learn about its human vision sensing solution that we have been developing for over 20 years through various conditions and environments. OMRON started developing at a time when people needed to adjust themselves to the machines, but the OKAO solution targeted to adjust machines to human. The Human Vision Sensing solution demonstrates high performance on various applications regardless of face type and the environment condition.

REGISTER TODAY

NOVEMBER WEBINAR:
WEATHER SENSOR

Save the date for our upcoming webinar on Thursday, November 16th, 2023 at 11:00am CST. Our speaker Cary Horan will be going over our Weather Sensor, and you won't want to miss it!

countdownmail.com

Interested in other events OMRON is a part of or hosting? Check out our events page so you never miss a thing!

Events Page
OMRON’S 300A, 1000VAC PCB RELAY – G9KA-E 
 

OMRON Membership Program

For a limited time, we will be offering our membership program free to anyone who signs up for it.

  • Free download of 2D/3D CAD and ECAD files
  • Updated information on New Products
  • Access to Omron's exclusive newsletter
  • Downloadable RoHS Certifications
  • Reference History
  • And more to come...
Sign Up For Membership
 

 

View Component Insider Archive:

 

August 2023 | July 2023  | June 2023 | April 2023 | March 2023 | February 2023 |
December 2022 | July 2022 | April 2022 | March 2022 | February 2022 |
January 2022

 

 Visit Our Website 
LinkedInTwitterInstagramYouTube