View as Webpage

February 2023 EDITION

 

Hello [First Name] !

Thanks for reading the February 2023 edition of Omron Electronic Component's product newsletter, Component Insider.

If you have any feedback on this new resource, please email us!

 

Sincerely,

The Team @ Omron Electronic Components

 

Featured New Products 

G3VM-WR

 

The WR series comes in Omron’s new P-SON package. They have a terminal shape that improves the stability of solder and offers better solder visibility. The output terminal pad has been expanded to allow higher current within the small package. The WR series supports 30V, 60V, 100V, and 200V load applications

 Learn More 

G3VM-401/601 AY2/DY2

 

These MOS FET relays offer greater capability than existing models in this AY/DY series. The 401AY2/DY2 and 601AY2/DY2 have a high dielectric strength of up to 5kV and a greater operating temperature range of up to 110 degrees Celsius.

 Learn More 

G3VM-41UR4

 

These MOS FET relays offer greater capability than existing models in the UR series. The G3VM-41UR4 has low off-state capacitance and low-ON-resistance and has a greater operating temperature range of up to 110 degrees Celsius. 

 Learn More 

B5W-LB

 

A new iteration of the light convergent sensor improves upon existing capabilities and connection with control boards including an indicator lamp to recognize an object is being sensed.

This sensor provides users with a reliable and efficient way to detect objects in a variety of materials; dark, light, transparent, or reflective.

 Learn More 

B5W-DB

 

This sensor expands the current B5W Sensor Lineup offering a variable sensing distance version capable of detecting objects up to over half a meter away when used with an external limiting resistor. The B5W Sensor has been a key component for object detection applications and touchless switches.

 Learn More 

D2GW

Bent Lever Models

 

The D2GW Sealed Ultra Subminiature Basic Switch is the industry’s smallest class size (8.3 x 6.5 x .3mm), which has a volume ratio that is 62% of the conventional types. The D2GW is an ideal switch solution for EV charging stations, electronic locks, metering devices, security devices, and more. To further expand the flexibility of installation, newly added bent lever models have been added to the lineup.

 Learn More 

High Performance Switches
for the Esports Gaming Industry

Sorry, you missed it!  You can still check out our last week’s webinar below to learn more about the latest switching technologies catered to performance in the Esports Gaming Industry. See how these switches can elevate your products and enable consumers and Esports professionals to perform at the highest level. Evan Kuhn, Business Development Manager, will be going in-depth on the following switch products:

• D2FP Optical Switches for Mice
• D2FC Micro Switches for Mice
• D2LS Ultra Subminiature Basic Switches for Mice    and Controllers 

WATCH ON-DEMAND

 Upcoming OMRON Events 

We're currently planning more webinars for 2023. Watch out for updates in Component Insider.

 

In the meanwhile, check out our events on-demand anytime on our YouTube channel.

 View On-Demand Webinars 
 

OMRON Membership Program

For a limited time, we will be offering our membership program free to anyone who signs up for it.

  • Free download of 2D/3D CAD and ECAD files
  • Updated information on New Products
  • Access to Omron's exclusive newsletter
  • Downloadable RoHS Certifications
  • Reference History
  • And more to come...
Sign Up For Membership

 

View Component Insider Archive:

 

December 2022 | July 2022 | April 2022 | March 2022 | February 2022

January 2022 | December 2021 | November 2021 | October 2021 
September 2021 | August 2021 | July 2021 | June 2021

 

 Visit Our Website 
Linkedin Youtube Twitter